TPA3128D2输入信号的耦合电容(PIN4/PIN10)着大小有什么区别不,
我原来C61/C69用了1uF,输出功率只有3.8W,现改成10uF,输出可以达到15W.
规格书内26dB 对应阻抗30K INPUT电容 3.3uF
而实际 INPUT电容 要配置10uF 方能达到输出功率。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
3.3uF电容是什么电容类型?如果使用的陶瓷电容的话,那么在施加电压的时候电容量易损耗,也就是说您这里描述的用的10uF的电容实际相当于3.几uF的容量。