This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3130 元器件选型

TI工程师你好,我们用TPA3130设计了一个功放板,双喇叭输出,喇叭是8OHM 15W喇叭,供电电压为15V。现在遇到的问题是音量开到最大时芯片和LC电感发热。

问题:

1、LC滤波电路中的22UH电感采用什么材质类型的电感,满足双喇叭30W输出的话,需要多大的线径,多大的电流?

2、0.68uF的电容建议用什么材质的电容,耐压多少伏,我们现在用的是X7R的0603贴片电容,网上有人用高频电容,直插的,推荐哪种,对发热有改善吗?

3、TPA3130全功率输出的情况,标准的双路输出电流在多少A?

4、我们用温度探头测到的温度最高到55度(开放环境下),这个温度长时间使用会有影响吗?