Other Parts Discussed in Thread: TAS5342
TI工程师,你好今天我用了你们的TAS5342芯片,那个RESET脚是由单片机控制的,开机的时候单片机给它一个3V的高电平,但是会出现POP声,请问如何解决这个难题。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TAS5342
TI工程师,你好今天我用了你们的TAS5342芯片,那个RESET脚是由单片机控制的,开机的时候单片机给它一个3V的高电平,但是会出现POP声,请问如何解决这个难题。
您好,请问您设置的是什么输出方式,单端还是差分。方便将原理图贴出来么。
最简单的解决问题是在后端加一个静音电路,使用三极管搭建,用MCU的IO进行控制。
你好:
有测过那个偏置的电压FL_OUT与FR_OUT是否与实际的输出的中点电压是否有偏差吗?
您好,
Pop音有两点建议:1)使用TI配套的PWM处理器TAS5508/18/38/48系列,会有专用的Valid引脚用于连接TAS5342的RST,防止pop;2)SE接法时,使用运放来生成、驱动重点电位,参考图如附件。
FM干扰应该是是系统layout所引起的电磁干扰问题,可从系统级角度进行优化。TAS5342是PWM功放,其PWM频率是有前级PWM处理器决定的,TAS5342处可以做的是尽量优化TAS5342的PCBlayout(规格书中有详细的建议),这样会对系统性能有一定的贡献。