This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5705 输入信号采样率切换问题

Other Parts Discussed in Thread: TAS5705

各位高手指点一下,遇到个问题。我是在自己的板子上调试的,用的是tas5705,输入信号MCLK=24.576MHZ,BCLK=64 LRCK,LRCK=44.1/48/88.2/96/176.4/192KHZ,上电配置好以后可以出声音,但是我切换输入信号的采样率的时候就会出问题,出现噪音或者没声音或者完全是噪音,如果是隔几分钟切换一下很少出现这样的问题,感觉就是不稳定。我觉得可能是配置顺序或者是电路图有问题,本人新手还望指教,谢谢。

配置顺序是上电后reset=0, 延时20ms,rest=1,延时20ms,然后通过iic配置寄存器 顺序是(0x1b=0x00) (0x03=0xA0)(0x04=0x05)(0x06=0x00)(0x07=0x30)(0x0E=0x30)(0x10=0x02)(0x19=0x30)(0x1A=0x0A)(0x11=0xB8)(0x12=0x60)(0x13=0xA0)(0x14=0x48)(0x17=0x00)(0x05=0x00)(0x20=0x0089777A)其他的都没配置,采用了默认值,上面这些有好多也是设置的默认值