请问是否是因为供电电压过大?改为15V之后似乎是没有出现这个问题。
我们现在想用一片TPA3130输出15W*2同时另外一片TPA3118输出40W*1,电源该如何选择?多少V多少A呢?
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问是否是因为供电电压过大?改为15V之后似乎是没有出现这个问题。
我们现在想用一片TPA3130输出15W*2同时另外一片TPA3118输出40W*1,电源该如何选择?多少V多少A呢?
谢谢
Hi,
我们现在使用的TPA3130,不是TPA3118哦。也可以20V供电吗?
应该测试哪个点的波形呢?
我们还没有测量波形,只是直观的看到喇叭停止振动。我们现在用的8欧姆的喇叭。
Hi,
感谢回复,现在使用15V供电,喇叭的阻抗是4欧姆左右(之前说8欧姆是错的)。
请问3130和3118还有3116都是看一份datasheet,如何区分呢?3130最大30W,3118最大60W,3116最大100W是这样吗?
现在看来可能是功率超过了,喇叭的承受范围。这样会导致喇叭突然停止振动吗?