This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

aic3204的声音大小如何调节,TMS320C5517的开发板

Other Parts Discussed in Thread: TMS320C5517

Ki开发板用的是TMS320C5517
这是一段1KHz的正弦波音频信号,播放的时候声音太大,怎么调节音量大小,可不可以不减小幅值在程序里调。Gi有个问题就是C5517有两片AIC3204,可不可以在两个模块同时播放同一段声音
#include "stdio.h"
#include "evm5517.h"
extern Int16 AIC3204_rset( Uint16 regnum, Uint16 regval);
#define Xmit 0x20
/*
 *
 *  aic3204_tone_headphone( )
 *      Output a 1 kHz tone through the STEREO OUT jack
 *
 */
Int16 aic3204_tone_headphone( )
{
    /* Pre-generated sine wave data, 16-bit signed samples */
    Int16 sinetable[48] = {
        0x0000, 0x10b4, 0x2120, 0x30fb, 0x3fff, 0x4dea, 0x5a81, 0x658b,
        0x6ed8, 0x763f, 0x7ba1, 0x7ee5, 0x7ffd, 0x7ee5, 0x7ba1, 0x76ef,
        0x6ed8, 0x658b, 0x5a81, 0x4dea, 0x3fff, 0x30fb, 0x2120, 0x10b4,
        0x0000, 0xef4c, 0xdee0, 0xcf06, 0xc002, 0xb216, 0xa57f, 0x9a75,
        0x9128, 0x89c1, 0x845f, 0x811b, 0x8002, 0x811b, 0x845f, 0x89c1,
        0x9128, 0x9a76, 0xa57f, 0xb216, 0xc002, 0xcf06, 0xdee0, 0xef4c
    };
    Int16 j, i = 0;
    Int16 sample;
   
     /* Configure AIC3204 */
    AIC3204_rset(  0, 0x00 );      // Select page 0
    AIC3204_rset(  1, 0x01 );      // Reset codec
    AIC3204_rset(  0, 0x01 );      // Point to page 1
    AIC3204_rset(  1, 0x08 );      // Disable crude AVDD generation from DVDD
    AIC3204_rset(  2, 0x00 );      // Enable Analog Blocks
    /* PLL and Clocks config and Power Up */
    AIC3204_rset(  0, 0x00 );      // Select page 0
    AIC3204_rset( 27, 0x00 );      // BCLK and WCLK is set as i/p to AIC3204(Slave)
    AIC3204_rset(  4, 0x07 );      // PLL setting: PLLCLK <- BCLK and CODEC_CLKIN <-PLL CLK
    AIC3204_rset(  6, 0x08 );      // PLL setting: J
    AIC3204_rset(  7, 0 );         // PLL setting: HI_BYTE(D)
    AIC3204_rset(  8, 0 );         // PLL setting: LO_BYTE(D)
    /* For 48 KHz sampling */
    AIC3204_rset(  5, 0x92 );      // PLL setting: Power up PLL, P=1 and R=2
    AIC3204_rset( 13, 0x00 );      // Hi_Byte(DOSR) for DOSR = 128 decimal or 0x0080 DAC oversamppling
    AIC3204_rset( 14, 0x80 );      // Lo_Byte(DOSR) for DOSR = 128 decimal or 0x0080
    AIC3204_rset( 20, 0x80 );      // AOSR for AOSR = 128 decimal or 0x0080 for decimation filters 1 to 6
    AIC3204_rset( 11, 0x88 );      // Power up NDAC and set NDAC value to 8
    AIC3204_rset( 12, 0x82 );      // Power up MDAC and set MDAC value to 2
    AIC3204_rset( 18, 0x88 );      // Power up NADC and set NADC value to 8
    AIC3204_rset( 19, 0x82 );      // Power up MADC and set MADC value to 2
    /* DAC ROUTING and Power Up */
    AIC3204_rset(  0, 0x01 );      // Select page 1
    AIC3204_rset( 12, 0x08 );      // LDAC AFIR routed to HPL
    AIC3204_rset( 13, 0x08 );      // RDAC AFIR routed to HPR
    AIC3204_rset(  0, 0x00 );      // Select page 0
    AIC3204_rset( 64, 0x02 );      // Left vol=right vol
    AIC3204_rset( 65, 0x00 );      // Left DAC gain to 0dB VOL; Right tracks Left
    AIC3204_rset( 63, 0xd4 );      // Power up left,right data paths and set channel
    AIC3204_rset(  0, 0x01 );      // Select page 1
    AIC3204_rset( 16, 0x06 );      // Unmute HPL , 6dB gain
    AIC3204_rset( 17, 0x06 );      // Unmute HPR , 6dB gain
    AIC3204_rset(  9, 0x30 );      // Power up HPL,HPR
    AIC3204_rset(  0, 0x00 );      // Select page 0
    EVM5517_wait( 500 );           // Wait
    /* ADC ROUTING and Power Up */
    AIC3204_rset(  0, 0x01 );      // Select page 1
    AIC3204_rset( 52, 0x0C );      // STEREO 1 Jack
                                   // IN2_L to LADC_P through 40 kohm
    AIC3204_rset( 55, 0x0C );      // IN2_R to RADC_P through 40 kohmm
    AIC3204_rset( 54, 0x03 );      // CM_1 (common mode) to LADC_M through 40 kohm
    AIC3204_rset( 57, 0xC0 );      // CM_1 (common mode) to RADC_M through 40 kohm
    AIC3204_rset( 59, 0x00 );      // MIC_PGA_L unmute
    AIC3204_rset( 60, 0x00 );      // MIC_PGA_R unmute
    AIC3204_rset(  0, 0x00 );      // Select page 0
    AIC3204_rset( 81, 0xc0 );      // Powerup Left and Right ADC
    AIC3204_rset( 82, 0x00 );      // Unmute Left and Right ADC
    
    AIC3204_rset( 0,  0x00 );   
    EVM5517_wait( 200 );           // Wait
    
    /* I2S settings */
    I2S0_SRGR = 0x0015;
    I2S0_ICMR = 0x0028;    // Enable interrupts
    I2S0_CR   = 0x8012;    // 16-bit word, Master, enable I2S
    /* Play Tone */
    for ( i = 0 ; i < 5 ; i++ )
    {
        for ( j = 0 ; j < 1000 ; j++ )
        {
            for ( sample = 0 ; sample < 48 ; sample++ )
            {
                I2S0_W0_MSW_W = (sinetable[sample]/5) ;  // Send left sample
                I2S0_W0_LSW_W = 0;
                I2S0_W1_MSW_W = (sinetable[sample]/5) ;  // Send right sample
                I2S0_W1_LSW_W = 0;
                while((Xmit & I2S0_IR) == 0);          // Wait for interrupt
            }
        }
    }
    /* Disble I2S */
    I2S0_CR = 0x00;
   
    return 0;
}