This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,
我在设计一个电路,需要得到输入的模拟信号的频率,有300Hz的,1500Hz的还有2300Hz的,这几个信号可以通过AUDIO CODEC 的ADC,然后求得输入信号的频率是多少吗? 应该怎样求得?用TI的哪款芯片可以实现该功能?
谢谢!
您好,是想检测到未知模拟信号的频率么?AIC3254内部的DSP可以实现频谱分析,结合外部MCU可以实时读取当前信号频谱分布。