This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3116D2 BTL模式喇叭损坏问题



喇叭1  - 4R 额定20W,最大25W

喇叭2 - 4R 额定30W,最大60W(规格书标称)

输入电阻26.6kohms+输入电容1uf-----INPR

GND ---1uF -----------                          INNR

输入电阻26.6kohms+输入电容1uf-----INPL

GND ---1uF -----------                          INNL

Table 1. Gain and Master/Slave

Gain 32 dB (R1)39 kΩ (R2)100 kΩ

输入电压:13.72V

LC 10uH+0.68uF

音频输入源 微型投影机接口,最大音量,检测音频的最大Vp-p= 1.9V peak-to-peak

试音 rock music后,喇叭突然出现停止发声,用手下按锥盆,又开始发声(3个喇叭都是这个问题),

检测FAULTZ pin  (11.79V)

测试输出的瞬时Vpeak电压,播放rock music时,瞬时Vpeak高达25V以上。

11/5之前的写的Vp-p不对,是瞬时Vpeak电压

请问这是导致喇叭损坏的原因吗?如何处理呢?

输入电压13.72V,输出瞬时Vpeak为何可以达到25V以上?