在看TPA6132A2与TLV320AIC3256时,对于耳机的参考地有一些疑问。请问在10.3提到耳机接头的GND必须单独接到SGND,请问HPVSS与SGND在IC内是连接在一起的吗,还是像TLV320AIC3256的Simplified Block Diagram 中的GND_Sense那样,是一种反馈。如果耳机的这个参考地直接接到主板上的地是否导致IC输出的音频HPL,HPR信号,耳机无法正常识别出来或导致其它问题?谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在看TPA6132A2与TLV320AIC3256时,对于耳机的参考地有一些疑问。请问在10.3提到耳机接头的GND必须单独接到SGND,请问HPVSS与SGND在IC内是连接在一起的吗,还是像TLV320AIC3256的Simplified Block Diagram 中的GND_Sense那样,是一种反馈。如果耳机的这个参考地直接接到主板上的地是否导致IC输出的音频HPL,HPR信号,耳机无法正常识别出来或导致其它问题?谢谢
Peng Qiu 说:在看TPA6132A2与TLV320AIC3256时,对于耳机的参考地有一些疑问。请问
在10.3提到耳机接头的GND必须单独接到SGND,请问HPVSS与SGND在IC内是连接在一起的吗,还是像TLV320AIC3256的Simplified Block Diagram 中的GND_Sense那样,是一种反馈。如果耳机的这个参考地直接接到主板上的地是否导致IC输出的音频HPL,HPR信号,耳机无法正常识别出来或导致其它问题?谢谢