This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,我们现在用TPA3110来驱动10W喇叭,目标是通过R11和R9将功放输出功率调高。
当前状态,测得V_PLIMIT=1.24V,然后我尝试将 R9更换为 3K 测得V_PLIMIT=2.53V
然后测试输出脚(OUTL+&OUTL-)得出波形如下方所示:
奇怪的是,不论我R9是1K还是3K,输出端测到的波形始终都是那样,没有变化。实际听喇叭的声音似乎也没有改变。通过控制调节音量大小, 波形也没有变化。请问这种现象是否正常?我还应该测量哪些参数更有利于调试?