TAS5631DKD的输出模式已配置成4×SE模式,/SD和/OTW引脚都通过一个10kohm电阻上拉到3.3V,芯片工作时/SD引脚输出高电平,外接的指示灯不亮,但/OTW引脚时钟输出低电平,外接的指示灯常亮,且功率级输出正常,已检查实际温度并没有过温,请问这个过温警告是什么原因导致呢?如果是欠压或过载导致的,那么应该如何调整电路,谢谢!
另外再问一下,目前我们的功放设计是基于TAS5631DKD和TAS5518C,但是已不推荐在新设计中使用,如果想把方案替换成新的TAS5631B和TAS5508C,在电路原理图上有需要修改的地方吗,可否直接将芯片替换?