Other Parts Discussed in Thread: TPA3112D1
我用TPA3112D1做了快板,测试时用的12V电压没啥问题,可我用18V电压时把PVCC与AVCC(7脚)之间的的10欧电阻烧坏,用万用表测量,发现14脚与地相通,我是参照评估板做的,评估板的资料与IC资料有一个地方不同,就是AVCC与14脚有一个100K的电阻,求解决方法?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TPA3112D1
我用TPA3112D1做了快板,测试时用的12V电压没啥问题,可我用18V电压时把PVCC与AVCC(7脚)之间的的10欧电阻烧坏,用万用表测量,发现14脚与地相通,我是参照评估板做的,评估板的资料与IC资料有一个地方不同,就是AVCC与14脚有一个100K的电阻,求解决方法?
您好
评估板使用手册和IC规格书中的描述是一致的,PVCC和AVCC之间的电阻均是10ohm/1206封装/ 1/4W。这个电阻你使用的封装是多大的?
我也是用的1206封装10欧姆的电阻,IC规格书中14脚是有一个100K电阻连接的,而评估板使用手册中两个AVCC是直接连在一起的,
你好,
请参考规格书:
The voltage slew rate of the gain terminals, along with terminals 1 and 14, must be restricted to no more than 10V/ms. For higher slew rates, use a 100kΩ resistor in series with the terminals.
对于这个问题,要么降低电压的slew rate,要么在14脚串接100k电阻。