This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3255,GVDD电压供应问题

Other Parts Discussed in Thread: TPA3255, TPA3255-Q1

您好!

在TPA3255以及TPA3255-Q1的datasheet中, GVDD电压供应部分有些不大懂。  在3255EVM中,中电压供应是12V没有歧义。而TPA3255-Q1的GVDD电压要求是10.6V,也就是说不能用12V的电压去供应。 而具体如何输入这一路电压,不是很明白。对于TPA3255-Q1,是否可以直接在GVDD和GND接电容而不用输入10.6V供电,只输入PVDD电压呢?

另外,我并没有使用外部控制器控制 /RESET 脚,要达到上电始终自动工作的功能,是否可以将/RESET脚和DVDD连接实现开机工作呢? 因为实验发现,悬空/RESET脚会导致不能正常工作。如果要设置/FAULT从低电位变为高电位后自动RESET,是否可以如TPA3128一样,将/RESET和/Fault连接,在用100k的电阻上拉到DVDD呢?

此外,C_Start脚连接的电容偏大是否只是会造成开机启动速度变慢的问题,而不会对正常工作造成影响呢?

盼复。

  • GVDD_X and PVDD_X represent a full bridge gate drive or power supply. GVDD_X is GVDD_AB or GVDD_CD. PVDD_X is PVDD_AB
    or PVDD_CD

    要求 GVDD_X to GND    9.8~ 11.4 V

    驱动能力: 50% duty cycle 44mA

    建议要单独的电源提供, 可以用 LDO 实现

  • 您好,
    GVDD电压是TPA3255的H桥的门驱动电压(Gate-drive voltage),而PVDD是H桥的供电电压,可以看下TPA3255-Q1内部框图,GVDD和PVDD是两个不同功能的供电电压,供电范围也不一样:TPA3255-Q1的GVDD供电电压范围是9.8V~11.4V,典型值10.6V;PVDD典型值是51V。因此都需要按规格要求供电。
  • 您好,
    TPA3255的/RESET和/Fault管脚应该是不能像TPA3128一样连接的,TPA3255的/RESET有效(置低)会强制/Fault管脚置高的(Note that asserting RESET low forces the FAULT signal high, independent of faults being present)。若将/RESET和/Fault连接在一起,将reset置低的同时没法使FAULT置高,/RESET的输入和/Fault的输出是矛盾的。

    C_Start脚连接的电容应该是与输出电压的时序有关,与开机启动没关系。