在TPA3123 EVM说明书上, c16和c9(1uF)开路, 剩下c19和c20(0.68uF),我用2*0.1uF并联上0.47uF电容,但是无负载的情况下静态电流为80ma左右(带上负载也是),去掉这几个电容,不带负载静态电流正常了,但是带上负载后电流变为90ma左右,反而还升上去了,认真看了datasheet,但就是找不到原因,不会因为电容一点差异就导致这么大的变化吧,恳请专家指导!注:电源为10V,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在TPA3123 EVM说明书上, c16和c9(1uF)开路, 剩下c19和c20(0.68uF),我用2*0.1uF并联上0.47uF电容,但是无负载的情况下静态电流为80ma左右(带上负载也是),去掉这几个电容,不带负载静态电流正常了,但是带上负载后电流变为90ma左右,反而还升上去了,认真看了datasheet,但就是找不到原因,不会因为电容一点差异就导致这么大的变化吧,恳请专家指导!注:电源为10V,
你好,你是直接在EVM板上调整电容值的吗?你说的应该是0.1uf//0.1uf//0.47uf来代替0.68uf?能说明一下你的负载是多大吗?EVM板上应该是对应8Ω的配置,可以参看datasheet上的page15的table 4。
因为EVM板上是单端输出,还是先确认一下你的隔直电容,其次可以测量一下你之前的测试条件下,测试点TP5或者TP2对地阻抗有多大。最后,如果有0.68uf电容的话,可以换上去测试,如果没有,建议直接使用0.47uf电容看一下测试结果。
感谢flei的答复!非常感谢你提醒了我page15的table4,这才发现我的电感值用得不对,用得太小了,负载4Ω,换上33uH和0.47uF电容,正常了 同时想请教下这电感和电容具体是什么作用呢,谢谢~!