TAS5630B,ready管脚输出高电平,OTW1输出低,SD管脚输出低,OTW2输出高,clip输出低电平,芯片周围器件没问题,工作电压也没有问题,datasheet中写的SD:OTW1:OTW2为0 0 1,描述为过载或欠压并超温警告,,但实际上喇叭最大只有240W,选用PBTL模式,目前不知道是什么原因导致过载
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TAS5630B,ready管脚输出高电平,OTW1输出低,SD管脚输出低,OTW2输出高,clip输出低电平,芯片周围器件没问题,工作电压也没有问题,datasheet中写的SD:OTW1:OTW2为0 0 1,描述为过载或欠压并超温警告,,但实际上喇叭最大只有240W,选用PBTL模式,目前不知道是什么原因导致过载
这个芯片没有Thermal Pad,散热加的是大的散热片加风扇,散热应该不是问题,因为是40块板子中出现了5块,想解决这个问题,音频输出不存在问题,SD:OTW1:OTW2为0 0 1是断续的,例如0.5s 0 0 1 ,0.5s 1 1 0
有可能输出电感饱和导致过载,适当减小供电电压再看下,是否还有这个报警?
另外,输出电感最小值在Recommended Operating Conditions都有推荐,可参考下。
电压反复测试,喇叭接上后,并没有电压下降,并不存在欠压情况,但是不加负载SD:OTW1:OTW2依然存在0 0 1,不知道是哪里原因导致芯片表明过载了?
ready 信号监测并未拉低,上电时序上是MCU控制各个电压起来后5ms,reset拉高,,现在有几块板子有这种情况发生,其他板子是好的,已经找的无头绪了,周围器件都换了一遍了
目前是上电后不加音频信号:SD:OTW1:OTW2一直是0 0 1,在加了音频信号后出现SD:OTW1:OTW2依然是0 0 1,但是断续的,随着音频信号在变化,例如0.5s 0 0 1 ,0.5s 1 1 0,我感觉现在是芯片上电后就进入到一种异常状态样?