Other Parts Discussed in Thread: TAS5825M
各位好!
最近使用TAS5825初始化过程如下
1.上电
2.PDN = 1; //bring up PDN to High
3.DELAY 5MS
4.START sclk LRCLK
5.DELAY 5MS
6. 配置寄存器
W 0x98 0x00 0x00 //choose page0
w 0x98 0x01 0x11 //reset DSP and IIC REG
W 0x98 0x50 0x00 // no auto_mute
w 0x98 0x54 0x1f // again -11.5db
w 0x98 0x60 0x07 // gpio 0-2 output
w 0x98 0x61 0x0b //GPIO0 as FAULTZ output
w 0x98 0x62 0x09 //Auto mute flag for left channel
w 0x98 0x63 0x09 //Auto mute flag for right channel
7. w 0x98 0x03 0x02 // set the device into HiZ state and enable DSP
8.w 0x98 0x03 0x03 // set the device into PLAY state
这是按照手册配置的,我主控FS=96K IIS 24BIT ,但是TAS5825没有输出,请问大家这会是哪里出了问题呢?
还有就是步骤 7 中的DSP的使能对不对?请不吝赐教!