This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA6120A2做的耳放,居然输出100mv左右的直流,不知道哪里出了问题,求指教!

Other Parts Discussed in Thread: OPA1632, TPA6120A2, TAS5630B

 电路如上图,电路是一个4片6120并联的结构,图上只截取了之中之一。

使用opa1632输出差分信号给四片6120,每片6120使用单端输入的方式分别对正负差分信号进行放大输出,输出信号串联10R电阻后并联。

在不带负载,输入对地短路的情况下,经过示波器检测输出没有自激情况,正负输出端对地静态电压达到100mv左右,正负输出之间静态电压倒是很小几个mv。

虽然电路是差分信号输出,但在使用中也会去正负信号之一作为单端输出来用,所以100mv的电压是不合适的。

请问为什么输出端对地电压这么高,哪里出了问题,应该如何修改。

  • 您好,

    我感觉应该是TPA6120A2输出信号串联10R电阻后并联,这样会产生回流电路,回流电路的电流在10R电阻上产生的。建议断开其他路TPA6120A2输出信号,只测量其中一路TPA6120A2输出对地电压,看看电压是多少。
  • 感谢您的回复,昨天断开并联测了一下还是会有直流输出。我又测量了下前面的运放的信号,发现运放输入端和输出端有40mv左右的直流输出,不过输入信号在经过耦合电容之前直流分量是很小的只有1mv左右甚至更小。
    看来应该是opa1632部分有问题了,这个电路我参考的TAS5630B的EVM板上的电路形式做的,那个电路上Vcom是没接的,我给对地接了一个0.1uf的电容。这个Vcom是不是应该直接接地啊,还是说是其他地方的问题。
  • 是的,opa1632的VOCM管脚是输入控制管脚,控制输出共模电压的,在您的应用中需要接地。
  • 试了一下果然是这个的原因,现在输出直流只有9mv了,谢谢了
x 出现错误。请重试或与管理员联系。