This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear TI
我们使用的TPA3221在BTL模式下,如果接双声道的话不会有任何异常,但是在BTL模式下只接一个输出4欧姆的喇叭,在音源有高音部分的时候会出现一小段类似保护的声音。检测只接了一个负载输出电感的波形发现PWM波形会整体上移2V左右的幅值。请问我应该怎么解决这个问题?
tpa3221电路图.pdfdear ti
附件为原理图,烦请帮忙查阅,我再重复一下,我是做的BTL模式(扬声器有主副箱),供电电压为27.5V ,只接主箱的时候当声音稍微大一点就会出现卡顿的声音,用示波器检测输出电感前端的信号发现有当大信号来时占空比会减小和整体幅值上移2V。现在我将供电电压上升到32.5V的时候就不会出现这种情况,请问1.这是IC本身就会出现这种问题还是我设计出现了问题?2,我使用32.5V的供电电压在供电范围内是否会影响IC的使用?3.如果我的供电电压使用的是27.5V我该如何去解决这个问题?