This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5751调整输出功率

輸入是0 & -12dB 但是我輸出希望可以自動的維持在固定的輸出功率 ,能告诉怎么调节吗?

輸入0 跟-12dB 在PVDD12V 要求8欧8W喇叭,声音功率调整到7.5~8W之间,PVDD24V要求8欧10W喇叭声音功率调到9W

最大不失真功率7.5W+/-0.5W,AVL限定在8W+/-0.5W;功放24V,最大不失真功率9W+/-0.5W,AVL限定在10W+/-0.5W;