This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320DAC3101 喇叭/耳機 音量控制



在上次的提問中並沒有得到有效的幫助, 但也沒有了回應,所以再發一次,並附上了上次的連結!謝~

前端接上手机,降音量到50%左右,后端的喇叭基本就没有声音了,而耳机是正常的,请帮忙分析分析具体原因。

将音量调到100%是喇叭是正常的,总的来说,手机音量从100%到-60%这段区间下降很过于明显,到了50%基本没声音了,但耳机的音量都正常。

下面是我们这边对codec 寄存器的初始化配置:

{

//page 0

        { 0x00,Audio_I2C_W, 0x00 },//
        { 0x01,Audio_I2C_W, 0x01 },//s/w reset
        { 0x04,Audio_I2C_W, 0x07 },//PLL_clkin = BCLK,codec_clkin = PLL_CLK
        { 0x05,Audio_I2C_W, 0x94 },
        { 0x06,Audio_I2C_W, 0x07 },
        { 0x07,Audio_I2C_W, 0x00 },
        { 0x08,Audio_I2C_W, 0x00 },
        { 0x1B,Audio_I2C_W, 0x30 },//mode is i2s,wordlength is 16
        { 0x1C,Audio_I2C_W, 0x00 },//Data-Slot Offset Programmability 
        { 0x1D,Audio_I2C_W, 0x00 },
        { 0x1E,Audio_I2C_W, 0x00 },
        { 0x0B,Audio_I2C_W, 0x82 },//NDAC is powered up and set to 2
        { 0x0C,Audio_I2C_W, 0x87 },//MDAC is powered up and set to 7
        { 0x0D,Audio_I2C_W, 0x00 },//DOSR = 128, DOSR(9:8) = 0
        { 0x0E,Audio_I2C_W, 0x80 },//DOSR(7:0) = 128
        { 0x74,Audio_I2C_W, 0x00 },//DAC => volume control thru pin disable 
        { 0x44,Audio_I2C_W, 0x00 },//DAC => drc disable, th and hy
//     { 0x41,Audio_I2C_W, 0x0A },// DAC => 0 db gain left
        { 0x42,Audio_I2C_W, 0x0A },//DAC => 0 db gain right
//page 1
        { 0x00,Audio_I2C_W, 0x01 },
        { 0x21,Audio_I2C_W, 0x4E },
        { 0x1F,Audio_I2C_W, 0x06 },   //0xC6
        { 0x23,Audio_I2C_W, 0x44 },
        { 0x28,Audio_I2C_W, 0x06 },//Garlin_2019092001--     0x0E },
        { 0x29,Audio_I2C_W, 0x06 },//Garlin_2019092001--     0x0E },
        { 0x24,Audio_I2C_W, 0x00 },
        { 0x25,Audio_I2C_W, 0x00 },
        { 0x2E,Audio_I2C_W, 0x0B },
//     { 0x30,Audio_I2C_W, 0x40 },
//     { 0x31,Audio_I2C_W, 0x40 },
//page 0
        { 0x00,Audio_I2C_W, 0x00 },
        { 0x3C,Audio_I2C_W, 0x17 },           //             DAC Processing Block Selection           PRB_P23
//page 8
        { 0x00,Audio_I2C_W, 0x08 },
        { 0x01,Audio_I2C_W, 0x04 },
//page 0
        { 0x00,Audio_I2C_W, 0x00 },
        { 0x3F,Audio_I2C_W, 0xFE },
        { 0x40,Audio_I2C_W, 0x00 },
//page 1
        { 0x00,Audio_I2C_W, 0x01 },
        { 0x23,Audio_I2C_W, 0x08 },//44
        { 0x23,Audio_I2C_W, 0x00 },//44
        { 0x26,Audio_I2C_W, 0x00 }, //0xA1
        { 0x27,Audio_I2C_W, 0x00 }, //0XA1
        { 0x23,Audio_I2C_W, 0x40 },//44
        { 0x23,Audio_I2C_W, 0x44 },//44
        { 0x26,Audio_I2C_W, 0x00 }, //0xA1
        { 0x27,Audio_I2C_W, 0x00 }, //0XA1
        { 0x2A,Audio_I2C_W, 0x15 },//0x0B },
        { 0x2B,Audio_I2C_W, 0x15 },//0x0B },
//page 1
        { 0x00,Audio_I2C_W, 0x01 },
        { 0x2A,Audio_I2C_W, 0x0C },
        { 0x2B,Audio_I2C_W, 0x0C },
        { 0x20,Audio_I2C_W, 0xC6 },
//     { 0x24,Audio_I2C_W, 0x30 },
//     { 0x25,Audio_I2C_W, 0x30 },
//     { 0x31,Audio_I2C_W, 0x00 },
}

  • 前端接上手机,降音量到50%左右,后端的喇叭基本就没有声音了,而耳机是正常的,请帮忙分析分析具体原因。
    既然耳机是正常的,说明器件能够输出的。
    所以可能喇叭和耳机的响度和信号的非线性和特性不同引起的