This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC3106 HPOUT电压

Other Parts Discussed in Thread: TLV320AIC3106

TLV320AIC3106使用HPOUT驱动32Ω的喇叭,我们使用0dB数字音源,DAC to HPOUT增益配置为0, DAC Digital  Volume配置为0,测量HPOUT电压有效值为0.38Vrms左右,HPOUT和HPCOM之间差分电压为0.8Vrms左右,与手册描述的单端HPOUT输出0.707Vrms相去甚远。想问一下这个输出电压是不是正确的,还是说要把HPOUT Output Level Control配置成9dB才能输出到0.707Vrms,或是说有其他寄存器需要配置

  • 信号输出了, 应该说芯片工作没有什么问题, 输出不同也许是输入信号, 0dB数字音源到端口的实际电压, 输入输出阻抗等影响的
  • 您好,0.707Vrms的测试条件是负载为16ohm的条件,您的负载是32ohm的。
    方便测试下16ohm负载的条件下,HPOUT的输出幅值是否和datasheet吻合吗?
x 出现错误。请重试或与管理员联系。