This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AIC3254 启动问题与延时调节功能实现过程

AIC3254 启动问题 :没有IIS,时钟是用MSP430产生的8M给AIC3254工作时钟的,但是每次启动要用手摸一下MCLK才能启动,什么原因呢!大侠们能否说明一下AIC3254启动过程。

另外需要功能调节延时,请问怎么实现? 目前已经实现固定的延时。谢谢!

  • 你好:

                 AIC3254的启动过程可参考附件的第87页和txt文档

                 你说的这种情况很奇怪,但是通常是由于配置AIC3254不正确所导致。请问你是如何配置AIC3254的?

                  此外你说的需要功能调节延时是需要用在哪里?您说在固件中的延迟已经实现是说Pure Path Studio中实现么?

  • HI Derek

    如何配置AIC3254,是由Pure Path Studio 产生main_Rate8.cfg ,按main_Rate8.cfg里面的顺序写命令的。

    另外MSP430写程序,这p1.1接AIC3254 的RESET引脚,P1.4产生一个8M的时钟给AIC3254给 MCLK 引脚。请问这两个引脚操作有什么注意的、?

     

  • 此外你说的需要功能调节延时是需要用在哪里?您说在固件中的延迟已经实现是说Pure Path Studio中实现么?

    补充:调节延时功能是MIC 的声音到耳机输出的延时,这样效果可助听器类似,外接一个按键做调节。 固定的延迟在Pure Path Studio中实现了,但是将更改为MCU+AIC3254自己做的PCB小板上出现用手接触一下才能有声音输出。暂时没有找到原因在哪,急急急!

  • 你好:

             由于Purepath下载后,会把Codec配置成默认的格式。他对PLL的配置的分频系数是按照MCLKC为4.096M的配置。并且会配置Codec为从模式。请问你的系统中,I2S时钟是外部提供的,还是Codec自己产生的。如果是外部提供仅需要修改AIC3254的分频器和PLL的配置。如果是自己产生,还需要将Codec配置从主模式,Power on BCLK。

     

  • 你好:

             如果是MIC进,Headphone出,那么Codec是主。

  •  如图,codec 时钟是 MCU产生8M 给MCLK

    配置如下:

    #   --------------------------------------------------------------- page 0 is selected
    w 30 00 00
    #   # reg[  0][  1] = 0x01 ; Initialize the device through software reset
    > 01
    #   --------------------------------------------------------------- page 1 is selected
    w 30 00 01
    #   # reg[  1][  1] = 0x08 ; Disable weak AVDD to DVDD connection
    > 08
    #   # reg[  1][  2] = 0x00 ; Enable Master Analog Power Control
    > 00
    #   # reg[  1][ 71] = 0x32 ; Set the input power-up time to 3.1ms
    w 30 47 32
    #   # reg[  1][123] = 0x05 ; Force REF charging time to 40ms
    w 30 7b 05
    #   --------------------------------------------------------------- page 8 is selected

    省略中间 一起写完

    #   --------------------------------------------------------------- page 166is selected

    后面再写配置

    #   --------------------------------------------------------------- page 0 is selected
    w 30 00 00
    #   # reg[  0][ 60] = 0x00 ; Use miniDSP_D for signal processing
    w 30 3c 00
    #   # reg[  0][ 61] = 0x00 ; Use miniDSP_A for signal processing
    > 00
    #   # reg[  0][ 17] = 0x08 ; 8x Interpolation
    w 30 11 08
    #   # reg[  0][ 23] = 0x04 ; 4x Decimation
    w 30 17 04
    #   
    w 30 0f 03
    #   
    > 88
    #   
    w 30 15 03
    #   
    > 88
    #   --------------------------------------------------------------- page 8 is selected
    w 30 00 08
    #   # reg[  8][  1] = 0x04 ; adaptive mode for ADC
    > 04
    #   --------------------------------------------------------------- page 44 is selected
    w 30 00 2c
    #   # reg[ 44][  1] = 0x04 ; adaptive mode for DAC
    > 04
    #   --------------------------------------------------------------- page 0 is selected
    w 30 00 00
    #   # reg[  0][  5] = 0x91 ; P=1, R=1, J=24
    w 30 05 91
    #   # reg[  0][  6] = 0x18 ; P=1, R=1, J=24
    > 18
    #   # reg[  0][  7] = 0x00 ; D=0000 (MSB)
    > 00
    #   # reg[  0][  8] = 0x00 ; D=0000 (LSB)
    > 00
    #   # reg[  0][  4] = 0x03 ; PLL_clkin = MCLK, codec_clkin = PLL_CLK, PLL on
    w 30 04 03
    #   # reg[  0][254] = 0x0a ; Delay 10ms for PLL to lock
    w 30 fe 0a
    #   # reg[  0][ 12] = 0x88 ; MDAC = 8, divider powered on
    w 30 0c 88
    #   # reg[  0][ 13] = 0x03 ; DOSR = 768 (MSB)
    > 03
    #   # reg[  0][ 14] = 0x00 ; DOSR = 768 (LSB)
    > 00
    #   # reg[  0][ 18] = 0x02 ; NADC = 2, divider powered off
    w 30 12 02
    #   # reg[  0][ 19] = 0xb0 ; MADC = 48, divider powered on
    > b0
    #   # reg[  0][ 20] = 0x80 ; AOSR = 128
    > 80
    #   # reg[  0][ 11] = 0x82 ; NDAC = 2, divider powered on
    w 30 0b 82
    #   --------------------------------------------------------------- page 1 is selected
    w 30 00 01
    #   # reg[  1][ 51] = 0x40 ; Mic Bias enabled, Source = Avdd, 1.25V
    w 30 33 40
    #   # reg[  1][ 52] = 0x40 ; Route IN1L to LEFT_P with 10K input impedance
    > 40
    #   # reg[  1][ 54] = 0x40 ; Route CM1L to LEFT_M with 10K input impedance
    w 30 36 40
    #   # reg[  1][ 55] = 0x40 ; Route IN1R to RIGHT_P with 10K input impedance
    > 40
    #   # reg[  1][ 57] = 0x40 ; Route CM1R to RIGHT_M with 10K input impedance
    w 30 39 40
    #   # reg[  1][ 59] = 0x00 ; Enable MicPGA_L Gain Control, 0dB
    w 30 3b 00
    #   # reg[  1][ 60] = 0x00 ; Enable MicPGA_R Gain Control, 0dB
    > 00
    #   --------------------------------------------------------------- page 0 is selected
    w 30 00 00
    #   # reg[  0][ 81] = 0xc0 ; Power up LADC/RADC
    w 30 51 c0
    #   # reg[  0][ 82] = 0x00 ; Unmute LADC/RADC
    > 00
    #   --------------------------------------------------------------- page 1 is selected
    w 30 00 01
    #   # reg[  1][ 20] = 0x25 ; De-pop: 5 time constants, 6k resistance
    w 30 14 25
    #   # reg[  1][ 12] = 0x08 ; Route LDAC to HPL
    w 30 0c 08
    #   # reg[  1][ 13] = 0x08 ; Route RDAC to HPR
    > 08
    #   # reg[  1][ 14] = 0x08 ; Route LDAC to LOL
    > 08
    #   # reg[  1][ 15] = 0x08 ; Route LDAC to LOR
    > 08
    #   --------------------------------------------------------------- page 0 is selected
    w 30 00 00
    #   # reg[  0][ 63] = 0xd4 ; Power up LDAC/RDAC w/ soft stepping
    w 30 3f d4
    #   --------------------------------------------------------------- page 1 is selected
    w 30 00 01
    #   # reg[  1][ 16] = 0x00 ; Unmute HPL driver, 0dB Gain
    w 30 10 00
    #   # reg[  1][ 17] = 0x00 ; Unmute HPR driver, 0dB Gain
    > 00
    #   # reg[  1][ 18] = 0x00 ; Unmute LOL driver, 0dB Gain
    > 00
    #   # reg[  1][ 19] = 0x00 ; Unmute LOR driver, 0dB Gain
    > 00
    #   # reg[  1][  9] = 0x3c ; Power up HPL/HPR and LOL/LOR drivers
    w 30 09 3c
    #   --------------------------------------------------------------- page 0 is selected
    w 30 00 00
    #   # reg[  0][ 64] = 0x00 ; Unmute LDAC/RDAC
    w 30 40 00
    #   # reg[0][82] = 0
    w 30 52 00
    #   # reg[0][83] = 0
    > 00
    #   # reg[0][86] = 32
    w 30 56 20
    #   # reg[0][87] = 223
    > df
    #   # reg[0][88] = 0
    > 00
    #   # reg[0][89] = 104
    > 68
    #   # reg[0][90] = 168
    > a8
    #   # reg[0][91] = 6
    > 06
    #   # reg[0][92] = 0
    > 00
    #   # reg[0][84] = 0
    w 30 54 00
    #   # reg[0][94] = 32
    w 30 5e 20
    #   # reg[0][95] = 223
    > df
    #   # reg[0][96] = 0
    > 00
    #   # reg[0][97] = 104
    > 68
    #   # reg[0][98] = 168
    > a8
    #   # reg[0][99] = 6
    > 06
    #   # reg[0][100] = 0
    > 00

  • 你好:

    PPS 中的cfg配置是针对MCLK为4.096MCLK配置的,并且是从模式。现在您需要修改时钟和I2S格式,Codec的PLL中的系数R ,J, D,P.  Dividers中的NDAC, NADC MDAC,MADC,DSOR,ASOR。 I2S 接口配置BCLK direction, WCLK direction, BDIV_CLKIN.

  • 能否详细说明一下,如上怎样改正?

  • 你好:

               PLL修改该三个寄存器:

    #   # reg[  0][  6] = 0x0C ; P=1, R=1, J=12
    w 30 06 0C
    #   # reg[  0][  7] = 0x0B ; D=2880 (MSB)
    w 30 07 0B 40
    #   # reg[  0][  8] = 0x40 ; D=2880 (LSB)

               I2S格式需要修改的寄存器:

    #   # reg[  0][ 27] = 0x0C ; BCLK and WCLK Output
    w 30 1B 0C
    #   # reg[  0][ 29] = 0x01 ; BDIV_CLKIN = DAC_MOD_CLK
    w 30 1D 01
    #   # reg[  0][ 30] = 0x8C ; Power ON BCLK Divider
    w 30 1E 8C

     

  • 谢谢Derek 问题已经解决!

  • DEREK 您好!

    打扰您!我在使用AIC3204时遇到很奇怪的问题。我希望配置3204为主模式,输出BCLK和WCLK, 使用了别的MCU, 控制程序用了usbstk5505的例程中的aic3204_loop_linein()和aic3204_tone_headphone( ),反复检查硬件,与usbstk5505完全一致。MCU操作I2C写3204成功,可看到正确应答信号。(如将地址改为别的,就没有应答,MCU与3204应通信正常),MCLK用有源晶振10M, 但是我怎么也无法在BCLK和WCLK看到输出,已经调试1周无法解决,万望不吝赐教!程序如下:

    Int16 aic3204_tone_headphone( )
    {

        Int16 j, i = 0;
        Int16 sample;
        //if(!I2C_Init(AIC3204_IDENT_W)) //Write CMD addr=0x34,aic23 addrs
     //{return false;}
     //IdentAddr =0x30;
     I2C_Init(AIC3204_IDENT_W);
        
        /* Configure Serial Bus */
        //SYS_EXBUSSEL |= 0x0100;  // Configure Serial bus 0 for I2S0

        /* Configure AIC3204 */
        if(!AIC3204_rset( 0, 0 ))return false;      // Select page 0
        AIC3204_rset( 1, 1 );      // Reset codec
        AIC3204_rset( 0, 1 );      // Select page 1
        AIC3204_rset( 1, 8 );      // Disable crude AVDD generation from DVDD
        AIC3204_rset( 2, 1 );      // Enable Analog Blocks, use LDO power
        AIC3204_rset( 0, 0 );
        /* PLL and Clocks config and Power Up  */
        AIC3204_rset( 27, 0x0c );  // ori=d BCLK and WCLK are set as o/p; AIC3204(Master)
        AIC3204_rset( 28, 0x00 );  // Data ofset = 0
        AIC3204_rset( 4, 3 );      // PLL setting: PLLCLK <- MCLK, CODEC_CLKIN <-PLL CLK
        AIC3204_rset( 6, 5 );      // PLL setting: J=5;ORI=J=7
        //AIC3204_rset( 7, 0x0 );   // PLL setting: HI_BYTE(D=0)
        //AIC3204_rset( 8, 0x0 );   // PLL setting: LO_BYTE(D=0),
        //AIC3204_rset( 7, 0x06 );   // PLL setting: HI_BYTE(D=1680)
        //AIC3204_rset( 8, 0x90 );   // PLL setting: LO_BYTE(D=1680),
                                   //NOW J.D=5.0, PLL=36.864M/2*5=92.16M,ADC_MOD_CLK=92.16M/15=6.144M, /128=48KHZ
                                   //ORI= J.D=7.168, PLL=12M*7.168=86.016M,ADC_MOD_CLK=86.016M/14=6.144M, /128=48KHZ
        AIC3204_rset( 29, 0x80 );                          
        AIC3204_rset( 30, 0x84 );  // For 32 bit clocks per frame in Master mode ONLY
                                   // BCLK=DAC_CLK/N =(12288000/8) = 1.536MHz = 32*fs
        AIC3204_rset( 5, 0xA1 );   // PLL setting:0XA1=P=2 and R=1; ORI=0X91=Power up PLL, P=1 and R=1
        AIC3204_rset( 13, 0 );     // Hi_Byte(DOSR) for DOSR = 128 decimal or 0x0080 DAC oversamppling
        AIC3204_rset( 14, 0x80 );  // Lo_Byte(DOSR) for DOSR = 128 decimal or 0x0080
        AIC3204_rset( 20, 0x80 );  // AOSR for AOSR = 128 decimal or 0x0080 for decimation filters 1 to 6
        AIC3204_rset( 11, 0x83 );  // Power up NDAC and set NDAC value to 3,ORI=2
        AIC3204_rset( 12, 0x85 );  // Power up MDAC and set MDAC value to 5,ORI=7
        AIC3204_rset( 18, 0x85 );  // Power up NADC and set NADC value to 5,ORI=7
        AIC3204_rset( 19, 0x83 );  // Power up MADC and set MADC value to 3,ORI=2
        /* DAC ROUTING and Power Up */
        AIC3204_rset( 0, 1 );      // Select page 1
        AIC3204_rset( 0x0c, 8 );   // LDAC AFIR routed to HPL
        AIC3204_rset( 0x0d, 8 );   // RDAC AFIR routed to HPR
        AIC3204_rset( 0, 0 );      // Select page 0
        AIC3204_rset( 64, 2 );     // Left vol=right vol
        AIC3204_rset( 65, 0);      // Left DAC gain to 0dB VOL; Right tracks Left
        AIC3204_rset( 63, 0xd4 );  // Power up left,right data paths and set channel
        AIC3204_rset( 0, 1 );      // Select page 1
        AIC3204_rset( 0x10, 0x00 );// Unmute HPL , 0dB gain
        AIC3204_rset( 0x11, 0x00 );// Unmute HPR , 0dB gain
        AIC3204_rset( 9, 0x30 );   // Power up HPL,HPR
        AIC3204_rset( 0, 0 );      // Select page 0
        //USBSTK5505_wait( 100 );    // wait
        Delayms(100);
        /* ADC ROUTING and Power Up */
        AIC3204_rset( 0, 1 );      // Select page 1
        AIC3204_rset( 0x34, 0x30 );// STEREO 1 Jack
                             // IN2_L to LADC_P through 40 kohm
        AIC3204_rset( 0x37, 0x30 );// IN2_R to RADC_P through 40 kohmm
        AIC3204_rset( 0x36, 3 );   // CM_1 (common mode) to LADC_M through 40 kohm
        AIC3204_rset( 0x39, 0xc0 );// CM_1 (common mode) to RADC_M through 40 kohm
        AIC3204_rset( 0x3b, 0 );   // MIC_PGA_L unmute
        AIC3204_rset( 0x3c, 0 );   // MIC_PGA_R unmute
        AIC3204_rset( 0, 0 );      // Select page 0
        AIC3204_rset( 0x51, 0xc0 );// Powerup Left and Right ADC
        AIC3204_rset( 0x52, 0 );   // Unmute Left and Right ADC
       
        AIC3204_rset( 0, 0 );   
        //USBSTK5505_wait( 200 );  // Wait
        Delayms(100);

    }