This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320DAC3101的耳机插拔检测和耳机按钮检测

Other Parts Discussed in Thread: TLV320DAC3101

TLV320DAC3101 的规格书中,39页介绍到该料可以实现耳机插拔检测和耳机按钮检测:

1.不知道耳机插拔检测的具体原理如何实现的,规格书中没细说?

2.耳机按钮检测是否可以检测多个按钮,比如接听\挂断、音量+、音量-?

帮忙解答下,谢谢!

  • 您好,耳机插拔检测和按钮检测,可以参考Table6-21中具体寄存器的描述。

    The device not only detects a headset insertion event, but also is able to distinguish between the different headsets inserted, such as stereo headphones or cellular headphones. After the headset-detection event, the user can read page 0 / register 67, bits D6–D5 to determine the type of headset inserted.

    关于耳机按钮检测, 通过DAC 中断寄存器Register 44来的bit5来检测,它检测的只是是否有按钮press。所以我理解的是不论是音量,还是挂断接听按钮,都能检测。

  • 文档的示意图,为什么VOL/MICDET需要接地?是不是画错了,该怎么接才能实现耳机插拔检测呢,如果我使用的是带mic的美标耳机的话。