This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

紧急求助! 关于AIC3204的BCLK和WCLK输出的问题

TI的工程师您好!

我在使用AIC3204时遇到很奇怪的问题(AIC23B正常)。我希望配置3204为主模式,输出BCLK和WCLK, 使用了别的MCU, 控制程序用了usbstk5505的例程中的aic3204_loop_linein()和aic3204_tone_headphone( ),反复检查硬件,与usbstk5505完全一致。MCU操作I2C写3204成功,可看到正确应答信号。(如将地址改为别的,就没有应答,故判断MCU与3204应通信正常),MCLK用有源晶振10M, 但是我怎么也无法在BCLK和WCLK看到输出,已经调试1周无法解决,万望各位不吝赐教!程序如下,请帮忙看看是否有错误。以下主要是配置AIC3204,没有I2S数据收发部分。我理解只要配置完就应该在BCLK和WCLK测到输出波形,是这样吧?

Int16 aic3204_tone_headphone( )
{

    Int16 j, i = 0;
    Int16 sample;
     I2C_Init(AIC3204_IDENT_W);
    
    /* Configure Serial Bus */
    //SYS_EXBUSSEL |= 0x0100;  // Configure Serial bus 0 for I2S0

    /* Configure AIC3204 */
    if(!AIC3204_rset( 0, 0 ))return false;      // Select page 0
    AIC3204_rset( 1, 1 );      // Reset codec
    AIC3204_rset( 0, 1 );      // Select page 1
    AIC3204_rset( 1, 8 );      // Disable crude AVDD generation from DVDD
    AIC3204_rset( 2, 1 );      // Enable Analog Blocks, use LDO power
    AIC3204_rset( 0, 0 );
    /* PLL and Clocks config and Power Up  */
    AIC3204_rset( 27, 0x0c );  // ori=d BCLK and WCLK are set as o/p; AIC3204(Master)
    AIC3204_rset( 28, 0x00 );  // Data ofset = 0
    AIC3204_rset( 4, 3 );      // PLL setting: PLLCLK <- MCLK, CODEC_CLKIN <-PLL CLK
    AIC3204_rset( 6, 5 );      // PLL setting: J=5;ORI=J=7
    //AIC3204_rset( 7, 0x0 );   // PLL setting: HI_BYTE(D=0)
    //AIC3204_rset( 8, 0x0 );   // PLL setting: LO_BYTE(D=0),
    //AIC3204_rset( 7, 0x06 );   // PLL setting: HI_BYTE(D=1680)
    //AIC3204_rset( 8, 0x90 );   // PLL setting: LO_BYTE(D=1680), 
                     AIC3204_rset( 29, 0x80 );                          
    AIC3204_rset( 30, 0x84 );  // For 32 bit clocks per frame in Master mode ONLY
                               // BCLK=DAC_CLK/N =(12288000/8) = 1.536MHz = 32*fs
    AIC3204_rset( 5, 0xA1 );   // PLL setting:0XA1=P=2 and R=1; ORI=0X91=Power up PLL, P=1 and R=1
    AIC3204_rset( 13, 0 );     // Hi_Byte(DOSR) for DOSR = 128 decimal or 0x0080 DAC oversamppling
    AIC3204_rset( 14, 0x80 );  // Lo_Byte(DOSR) for DOSR = 128 decimal or 0x0080
    AIC3204_rset( 20, 0x80 );  // AOSR for AOSR = 128 decimal or 0x0080 for decimation filters 1 to 6
    AIC3204_rset( 11, 0x83 );  // Power up NDAC and set NDAC value to 3,ORI=2
    AIC3204_rset( 12, 0x85 );  // Power up MDAC and set MDAC value to 5,ORI=7
    AIC3204_rset( 18, 0x85 );  // Power up NADC and set NADC value to 5,ORI=7
    AIC3204_rset( 19, 0x83 );  // Power up MADC and set MADC value to 3,ORI=2
    /* DAC ROUTING and Power Up */
    AIC3204_rset( 0, 1 );      // Select page 1
    AIC3204_rset( 0x0c, 8 );   // LDAC AFIR routed to HPL
    AIC3204_rset( 0x0d, 8 );   // RDAC AFIR routed to HPR
    AIC3204_rset( 0, 0 );      // Select page 0
    AIC3204_rset( 64, 2 );     // Left vol=right vol
    AIC3204_rset( 65, 0);      // Left DAC gain to 0dB VOL; Right tracks Left
    AIC3204_rset( 63, 0xd4 );  // Power up left,right data paths and set channel
    AIC3204_rset( 0, 1 );      // Select page 1
    AIC3204_rset( 0x10, 0x00 );// Unmute HPL , 0dB gain
    AIC3204_rset( 0x11, 0x00 );// Unmute HPR , 0dB gain
    AIC3204_rset( 9, 0x30 );   // Power up HPL,HPR
    AIC3204_rset( 0, 0 );      // Select page 0
    //USBSTK5505_wait( 100 );    // wait
    Delayms(100);
    /* ADC ROUTING and Power Up */
    AIC3204_rset( 0, 1 );      // Select page 1
    AIC3204_rset( 0x34, 0x30 );// STEREO 1 Jack
                         // IN2_L to LADC_P through 40 kohm
    AIC3204_rset( 0x37, 0x30 );// IN2_R to RADC_P through 40 kohmm
    AIC3204_rset( 0x36, 3 );   // CM_1 (common mode) to LADC_M through 40 kohm
    AIC3204_rset( 0x39, 0xc0 );// CM_1 (common mode) to RADC_M through 40 kohm
    AIC3204_rset( 0x3b, 0 );   // MIC_PGA_L unmute
    AIC3204_rset( 0x3c, 0 );   // MIC_PGA_R unmute
    AIC3204_rset( 0, 0 );      // Select page 0
    AIC3204_rset( 0x51, 0xc0 );// Powerup Left and Right ADC
    AIC3204_rset( 0x52, 0 );   // Unmute Left and Right ADC
   
    AIC3204_rset( 0, 0 );   
    //USBSTK5505_wait( 200 );  // Wait
    Delayms(100);

}

  • 你好:

             我将你的代码数据放到我们的EVM板上测试,发现你的PLL与Divider设置有问题。         

    这个系数是你们需要的吗?并且没有power on divider。

    还有就是你们的配置时序也有点问题。建议参考如下顺序:

       --------------------------------------------------------------- page 0 is selected
    w 30 00 00
    #   # reg[  0][  1] = 0x01 ; Initialize the device through software reset
    > 01
    #   --------------------------------------------------------------- page 1 is selected
    w 30 00 01
    #   # reg[  1][  1] = 0x08 ; Disable weak AVDD to DVDD connection
    > 08
    #   # reg[  1][  2] = 0x00 ; Enable Master Analog Power Control
    > 00
    #   # reg[  1][ 71] = 0x32 ; Set the input power-up time to 3.1ms
    w 30 47 32
    #   # reg[  1][123] = 0x05 ; Force REF charging time to 40ms
    w 30 7b 05

    #   --------------------------------------------------------------- page 0 is selected
    w 30 00 00
    #   # reg[  0][  5] = 0x91 ; P=1, R=1, J=24
    w 30 05 91
    #   # reg[  0][  6] = 0x18 ; P=1, R=1, J=24
    > 18
    #   # reg[  0][  7] = 0x00 ; D=0000 (MSB)
    > 00
    #   # reg[  0][  8] = 0x00 ; D=0000 (LSB)
    > 00
    #   # reg[  0][  4] = 0x03 ; PLL_clkin = MCLK, codec_clkin = PLL_CLK, PLL on
    w 30 04 03
    #   # reg[  0][254] = 0x0a ; Delay 10ms for PLL to lock
    w 30 fe 0a
    #   # reg[  0][ 12] = 0x88 ; MDAC = 8, divider powered on
    w 30 0c 88
    #   # reg[  0][ 13] = 0x03 ; DOSR = 768 (MSB)
    > 03
    #   # reg[  0][ 14] = 0x00 ; DOSR = 768 (LSB)
    > 00
    #   # reg[  0][ 18] = 0x02 ; NADC = 2, divider powered off
    w 30 12 02
    #   # reg[  0][ 19] = 0xb0 ; MADC = 48, divider powered on
    > b0
    #   # reg[  0][ 20] = 0x80 ; AOSR = 128
    > 80
    #   # reg[  0][ 11] = 0x82 ; NDAC = 2, divider powered on
    w 30 0b 82

     

  • 谢谢,问题解决。一是配置问题,另外是MCLK硬件连接问题,导致MCLK未送入。