This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5805 idle noise 和功率问题



我们测试TAS5805performance的时候,发现了以下两个问题

1,喇叭的idle noise非常大,约为-53dB,人耳可以明显的听到Noise。

2.播放扫频的时候,喇叭的功率会随着频率的升高而升高,我们设置的是10W,但是播放扫频文件时,最高可以达到25W,播放1K文件文件的时候就没有这个问题。

我们将EVM board的I2S,I2C和PDN,Fault信号跳接到我们板子上,就听不到Noise,也不会出现功率增大的问题。我们把寄存器的配置修改成和EVM一致,还是会

出现上面两种情况。

PVDD=13.5V, 喇叭为4ohm

麻烦看看可能是什么原因引起的这两个问题。谢谢!