Other Parts Discussed in Thread: PCM1794
TI的工程师您好!
1. 我们希望验证ADC,DAC的SNR和DR指标,可否推荐实际相应的测试方法?比如ADC,输入是满幅正弦波,输出是24BIT数字,怎么计算SNR和DR?
2. 有无ADC的差分输入的推荐电路?
多谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: PCM1794
TI的工程师您好!
1. 我们希望验证ADC,DAC的SNR和DR指标,可否推荐实际相应的测试方法?比如ADC,输入是满幅正弦波,输出是24BIT数字,怎么计算SNR和DR?
2. 有无ADC的差分输入的推荐电路?
多谢!
多谢 DEREK!
规格书上的指标我们注意到了。但出于对系统性能的评估需求,您可否给出一个不使用专用仪器,仅利用常规仪表和电脑软件来评估实际ADC,DAC的SNR/DR数据的方法?
另外一个问题,3204的Decimation Filter A 、B都可以工作在96K FS下,此时的信号通带带宽(,及可以采样的最高信号频率)是否为96K*0.39=37.4K? Decimation Filter C 的通带带宽却只有192K*0.11=21K,采样频率提高后通带带宽却变小了,是这样理解吗?为什么会这样设计呢?我们通常希望提高FS来提高可以采样的最高信号频率呀? 这里反而下降了。
对于DAC的SNR,可用交流毫伏表粗略测量。模拟的交流毫伏表价格应当在1K一下。
1. ADC SNR测试:ADC输出是数字信号,不妨找块高性能的DAC板,把ADC输出的数字音频信号输出给DAC,再测试模拟的输出。TI有高性能的DAC可选,比如PCM1794/2,PC1704等。其中PCM1794/2的SNR可达132dB,对于测试普通的ADC测试应当足够了。市面上有不少高性能的声卡采用的是PCM1794芯片,可选择一下。
2. 采样频率:你说的对,提高采样频率可以提高被采样信号的频率。但在音频领域,因为音频信号的频率上限是20KHz,提高采样频率的目的通常不是为了采样更高频率的信号,而是为了通过提高采样频率,配合noise shapping来提高信号的SNR等指标。AIC3204的Decimation filter的设计也是针对音频,在采样频率更高时,Filter C没有把通带的频率设定得比20KHz更高。
如果想采样更高频率的信号,可尝试AIC3254,考虑从ADC获取没有经过decimation的信号,用AIC3254自带的miniDSP,自己灵活地设计decimation filter。
Best Regards
Frank Pan