由于中秋节假期,帖子审批以及工程师回复将会有所延迟,敬请谅解。

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于TLV320AIC3254的6路录音问题

Other Parts Discussed in Thread: TLV320AIC3254, TLV320AIC3268, PCM6260-Q1, PCM6360-Q1

您好,请问下TLV320AIC3254具有6路的语音录制功能,请问下,可否生成6路完全独立的音频文件?由于每个拾音器是分别放置于不同的位置。谢谢。

  • 您好,
    您是要6路一起录吗,TLV320AIC3254只有2路ADC,实现不了6路一起录音。
  • 您好,如果我要实现6路或以上同时录音,需要使用哪一款芯片?
  • 您好,我看规格书AIC3268的datasheet上说他具有8个单端或4个全差分模拟输入
  • TLV320AIC3268内部也是集成了2路ADC,对6路信号同时录音需要6路ADC,您可以看下PCM6360-Q1和PCM6260-Q1。
    对于“可否生成6路完全独立的音频文件”,我再确认下。
  • 需要同时几路录音,就需要一个内部至少有几个ADC的音频ADC。许多音频ADC和编解码器具有多个输入口,但这些都会经过内部集成的MUX最终进入内部1个或2个或几个ADC。所以您需要使用内部集成6个或6个以上ADC的音频芯片。PCM6360-Q1或PCM6260-Q1都是集成了6个ADC,如果需要6路以上同时录音,我在TI官网没有找到合适的产品推荐给您。

    经向其他资深工程师确认,ADC本身不创建音频文件(.wav、.mp3等),它创建多通道音频串行输出,主机处理器将其转换为所需的输出格式。PCM6360-Q1或PCM6260-Q1的EVMs可以用来直接将音频录制到计算机程序中,像Audacity。这是通过AC-MB主板上的主机处理器完成的,主机处理器首先将来自PCM6260-Q1的音频串行输出(I2S、TDM等)转换为计算机可以识别的USB音频数据流,然后将其保存为不同的格式。