This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EVM5517上电后LOL,LOR用示波器看有奇怪的噪声

Other Parts Discussed in Thread: TPA2012D2, TMS320C5517

您好!

这边AIC3204的HPL,HPR输出正常,想修改为LOL,LOR输出,发现有问题。

然后查了一下,未写入程序,上电后,就在LOL和LOR口检测到这个奇怪的波形。该噪声因为峰峰值在9V左右,频率为550 KHz

其中AIC3204和TPA2012D2边上的跳线帽JP53~JP60是按照evm5517_Schematics.pdf中的默认状态接的

波形如下

我示波器线,一边接地,一边测LOL或LOR,都是方波波形,峰峰值就为9 V左右,两块evm5517都这样。