This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3118D2 温升估算

Other Parts Discussed in Thread: TPA3118D2, TPA3116D2

请问在TPA311XD2系列规格书中为什么TPA3118和TPA3116的RθJC(top)会相差那么大呢?

3116 为1.2℃/W

3118为17.2℃/W,

其次使用TPA3118D2评估板。在室温25℃,输入电压24V/1.4A,负载8欧,输出30W。是否可以根据公式Tj =  TA + (RθJA*Power),

25+(32.4*(24*1.4-30))估算此时结温Tj = 141.64℃?