ERROR: MiniDSP failed to change adaptive buffer, pending bit remains set, reset target.
出现这断错误,可能出现的问题点在哪里? 能够列出来,给我一些参考。实在是没有办法解决掉。TI中国区的工程师请帮助解决一下。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Derek,
EVM测试是通过的。断开EVM上的AIC3256芯片,用I2C连线到我的PCB上的AIC3256, 程序下载后,就会出现MINIDSP的上述错误。 target board选的是正确的,Adaptive 也是Enabled.
MiniDSP Cycles TIME 设定是0x40. 会是这个问题吗?
EVM 的MCLK: 11.29MHz, 我自己PCB上给的MCLK是晶振12MHz, 经过PLL配置以后,都是44.1KHz,这个应该没问题啊。
Zhang