This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS2505的I2S master mode使用

Other Parts Discussed in Thread: TAS2505

各位专家好:

我们目前有一个设计,由于host侧的I2S只支持slave模式,需要使用TAS2505的I2S master mode,请问TAS2505是否可以支持master模式?如果可以支持master,请问TAS2505的MCLK是否可以使用一颗cmos晶振提供?频率是多少最好?这样的设计是否可行?

  • 您好,TAS2505 即可以支持I2S主机模式,也可以支持I2S 从机模式。
    当I2S 主机模式时,MCLK作为输入,WCLK和BCLK作为输出。 WCLK和BCLK的主从模式可通过Page 0 / Register 27进行配置。 可以参考TAS2505 的应用指南:
    www.ti.com.cn/.../slau472.pdf
    MCLK的最大频率为50Mhz,选择多大频率要看实际应用,比如 MCLK = 11.2896 MHz,采样率 fS = 44.1 kHz。