Other Parts Discussed in Thread: TLV320ADC6140
以前使用的是模拟麦克风,使用两个4路输入的CODEC,I2S格式,为了保证时钟同步,后面使用FPGA进行同步采样,设计8麦克风阵列效果还可以。为了简化设计6140+8个PDM话筒,配置安装手册(手册上数字麦克风的接法有错误,SEL引脚应该一个接VCC,一个接GND),每个话筒输出都正常,但是加入算法后效果不好。我用示波器看了一下,PDM时钟输出都是同步的。就想问一下,PDM麦克风输出后加入芯片内部滤波器是不是并行处理的,如果使用TDM格式输出,采样的到8路信号是不是有延时,如果有的话怎么计算。另外,里面每个通道都有相位校准寄存器,如果要调整,该如何处理。另外,TLV320ADC6140采用的是从模式,任何时钟都是外部处理器提供的,每个声道的数据采集到都是正常的,就是加入阵列算法后效果没有原来模拟的好,怀疑是音频相位问题。