This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC3106EVM板mic输入、Line输入不能同时使用

Ti的专家,帮忙给个建议:

3106的评估板,mic输入、Line输入不能同时使用,音量无法调节到适合的状态,始终都是Line声音过大,覆盖了Mic的小信号,导致Mic的语音几乎消失了。并且背景噪声较大。

  • 你好:

              请问你是怎么配置我们的codec的,能否截图看下。

  • 风,

    Line in信号一般在几百mV~2Vrms之间。是大信号。

    Mic信号一般在几个mV之内,是微弱信号。二者不能简单的叠加。

    背景噪声估计是麦克风产生的。麦克的SNR在94dB声压级时才不到60dB。在普通60~70dB的声压下的信噪比才30个dB。为了提高麦克的信噪比,常用限制带宽的方法。环境噪声多为低频噪声,将mic的高通频率设置在100Hz以上,会滤除掉一部分环境噪声。高频也可做低通滤波,滤除掉一部分嘶嘶声,但同时声音质量会受到一些损伤,需要折中。

    Best Regards

    Frank Pan