This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3116D2 SD问题

Other Parts Discussed in Thread: TPA3116D2

这两天意外发现TPA3116D2在正常工作过程中,SD脚(电路上SD脚和FAULT脚连在一起)如果给一个5~30us的低脉冲(平时为高),会随机导致芯片增益减半。电路原本设置为26dB,master模式,减半后变成20dB,如果重新给SD脚一个时间更长的低脉冲,比如几个ms,增益就会恢复正常。猜测可能是TPA3116D2在SD脚为低电平时会采样gain脚的电压,根据该引脚的电压设置增益,如果复位时间太短会导致无法采样到gain脚的电压,或者说采样到的电压为0,所以增益就变成了20dB。请问是这样吗?这种现象是正常的吗?SD脚的低电平有没有最短时间要求?另外:芯片设置为BD-Modulation工作模式,正常工作时MUTE脚一直拉低。

  • 您好,
    SD脚您是指TPA3116D2的SDZ管脚吗,SDZ是Shutdown管脚,低电平有效,为低电平时输出高组态,高电平时音频功放正常输出
    低电平关断时间Turn-off time典型值为2us,电平阈值为≤0.8V
    高电平开启时间Turn-on time典型值10ms,电平阈值为≥2V
    5~30us的低脉冲或几个ms的脉冲,电平电压是多少,可以附上波形吗
  • 您好,上电期间 ,在电压起来至稳定之前,建议将SD一直拉低,等电压起来稳定之后,SD再拉高。
    建议附上您的电路看下呢。