请问各位高手,有没有最简单的时钟信号产生芯片?因为我之前使用AIC3254的时候是使用单片机的振荡器的时钟直接输入到AIC3254的MCLK端,现在有个项目,发现时钟线不能拉得太长,不然会对外部造成很大的干扰,而单片机又不能贴着AIC3254布局,我直接就蒙了。急求各位的回答啊,给推荐一个时钟信号发生芯片,尽量要最简单的,时钟信号频率要求为11.2896MHz,这是AIC3254的DEMO板所使用的MCLK频率。谢谢了,各位,急求,哭求哇。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问各位高手,有没有最简单的时钟信号产生芯片?因为我之前使用AIC3254的时候是使用单片机的振荡器的时钟直接输入到AIC3254的MCLK端,现在有个项目,发现时钟线不能拉得太长,不然会对外部造成很大的干扰,而单片机又不能贴着AIC3254布局,我直接就蒙了。急求各位的回答啊,给推荐一个时钟信号发生芯片,尽量要最简单的,时钟信号频率要求为11.2896MHz,这是AIC3254的DEMO板所使用的MCLK频率。谢谢了,各位,急求,哭求哇。
Hi, Tiger,
可以考虑使用Bclk作为内部PLL的时钟输入源或者选用PLL170X系列的音频时钟发生器。
BR.
最简单的PLL1705这款:http://www.ti.com/lit/ds/symlink/pll1705.pdf