最近买了AIC3254EVM-K,带USB口。按照user's guide的说明一步一步安装后,PC机不能识别该EVM,总找不到原因。特此请教软件安装、板上各插针座的连接等,还需特别注意的问题。谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
最近买了AIC3254EVM-K,带USB口。按照user's guide的说明一步一步安装后,PC机不能识别该EVM,总找不到原因。特此请教软件安装、板上各插针座的连接等,还需特别注意的问题。谢谢!
检查下J12, J21, J22, ,J23这几个插针是否连接好,USB-MODEVM和PC连接时,查看下LED灯D3,D4,D5,D7亮吗?
PC机设备管理器提示:AIC32x4 EVM ?
另外,所有LED都亮:D2, D3、D4、D5、D7,D8
Hi
在AIC3254EVM-K板子上有2个EEPROM。 一个是在主板上,一个是在AIC3254的板子上。Tas1020启动后会读EEPROM的地址,当另个地址一样的时候就会有问题。所以建议将主板上的SW2的A0A1A2全设为0。将AIC3254板子上的W13用跳线帽拔掉,即Tas1020就会读主板子上的EEPROM。如果还是连接不上,建议重新烧写EEPROM。按照下面的文档烧写。

Hi,
如楼上所说,母板与子板各有一个EEPROM给TAS1020B存放firmware,这两个EEPROM不能同时使用,TAS1020B只能识别地址为0x50(A0,A1,A2=0)的EEPROM并读取其中的firmware。
用户指南里说的是指使用子板上的EEPROM,所以母板上EEPROM的A0,A1,A2地址就要设为非0状态,但子板W13跳线(设定子板EEPROM地址)必须跳上。
使用母板EEPROM时,子板W13跳线必须断开,设定SW2 A0,A1,A2为0。
如果上述两个EEPROM的设置都无法识别,可能就是firmware坏掉了,请用Derek的方法重新烧写TAS1020B的firmware。
说的非常清楚。
二种方法已试过,均不能识别。马上重烧firmware。谢谢!