This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Description of test phenomena:
1、SDIN pin has no signal input.
2、LRCLK and SCLK signal input is normal.VR_DIG voltage 1.496V,GVDD voltage 5.10V,AVDD voltage 5.18V.The ripple was less than 12mV.
3、The impedance of SPK is 8 ohm.PVDD voltage 24V.
4、Adjusting gain has no effect on idle noise.
Amy Luo,您好:
我们这边每块板子复现现在还不太一样,都是人耳可听到的噪声,小的时候大约5dB,大的时候20-30dB;,PCB为四层板,第二层第三层都是地层;Hybird 和BD模式都有尝试,下面是同事手中板子的现象:
1. yh的板子: Hybrid模式,播放非静音或静音数据时,都会高概率出现持续的噪声,噪声有大有小。BD模式,暂未听到噪声,也没有电感发热现象。
2. xt的板子: Hybrid模式,播放非静音或静音数据时,都会低概率出现持续的噪声,噪声较小。BD模式,有电感发热现象,暂未听到噪声。
3. fm的板子(只测试了一次): Hybrid模式,启动后播放非静音或静音数据时,听到持续的较大噪声。BD模式,电感有发热现象,启动后播放非静音或静音数据时,暂未听到噪声。
4. yx的板子:Hybrid模式,启机后约播放静音数据50s出现滋滋声持续2s,之后就没有听到噪声。BD模式现象一样,电感没有发热。
以下是有噪声时,测得的喇叭单端波形。
开关频率您配置的是384KHZ是吗?那Loop Bandwidth配置的是多少,即register 83 -Register address 0x53h-D[6-5]配置的是什么值?在Hybrid调整模式下是需要Fsw (Switching Frequency) ≥ 4.2 × Loop Bandwidth