在只用一个BTL模式的时候,可否使用INPUT_A和INPUT_B组成差分音源输入,OUT_A和OUT_B输出?还是说只能在PBTL模式的情况下使用INPUT_A和INPUT_B组成差分音源输入?
如果只用一个BTL模式输出的时候,INPUT_C和INPUT_D怎么接?空接还是接GND?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,参考table1的mode selection, 输出1xBTL 的话, AB channel active,输入为2N,差分输入,所以AB为差分输入,那么不用的C和D input, 建议input _C接DVDD, input_D接地. 不用的输出端BST_C和BST_D和OUT_C和OUT_D的bootstrap 电容需要接, LCfilter可不接.