This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
影响TPA3138D2输出功率的因素有很多,比如芯片耐温、内部集成管子可以流过的最大电流等
在4Ω负载下,流过内部开关管的电流是比其他6Ω、8Ω负载下是大的,这样可能会烧掉管子
根据功率P=U^2/R,功率一样的情况下,R越小,电流越大;
比如P=10W,如果R=8Ω,则可计算出U约为8.9V,电流为1.1A
如果R=6Ω,则可计算出U约为7.7V,电流为1.3A
如果R=4Ω,则可计算出U约为6.3V,电流为1.6A
输出级开关管导通电阻Ron是一定的,流过开关管因为电流不一样,导通电阻发热功率也不一样,电流越大,发热功率越大(P=I^2*R)
虽然都是12V供电,输出功率相同,但是输出电压不同(8.9V、7.7V、6.3V),那么多余的电压就消耗在导通电阻Ron发热了,也因此9V供电做4Ω10W就不会过温。
同样的道理,相同的供电电压,输出功率越小,发热功率就越大,效率就越低
温度是多少,会不会过温保护,总的来说是需要看发热功率的。
- 不同功率同样电流对比
12伏供电,8欧姆,双通道10W,计算电流为1.12A,温度是78度
12V供电,4欧姆,双通道5W,计算电流为1.12A,温度是101度
结果: 同样电流下,温差还是挺明显
10W时,总的输入功率12V*1.12A=13.44W,那么发热功率为3.44W
5W时,总的输入功率12V*1.12A=13.44W,那么发热功率为8.44W,发热功率大,温度高
下面这种情况是一样的道理:
- 不同供电电压对比
12V供电,4欧姆,双通道10W,计算电流为1.58A,过温保护
9V供电,4欧姆,双通道10W,计算电流为1.58A,温度是120度