Part Number: TAS2553
你好,我用I2S模式,请问Register 0x03的DIN_SOURCE_SEL怎么填?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,如果您的DIN为 I2S 输入, 那么0x03 bit[7:5]=010, bit 5 配置为1 为PDM not selected。
关于bit3 DIN_SOURCE_SEL的这四种配置,我这边再确认下是否针对的输入为PDM 模式的。
您好,DIN_SOURCE_SEL这四种配置的含义为,所以不论是I2S输入还是PDM输入,这四种配置主要针对于选择在哪个声道进行播放:
00 = Muted, no data is played
01 = Only data content on the left channel is played
10 = Only data content on the right channel is played
11 = Mix of left and right channels is played