This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
About PCM6240-Q1, we have a detection issue:
Now we set the register 0x75 bit7 micbias_pdz: 0d = Power down MICBIAS and use outside LDO for MIC bias(8.5V), we found that PCM6240-Q1 can't detect the input open circuit.
The input open circuit detection condition needs to meet below:
Whether does internal MICBIAS must be used for input open circuit detection?
Best Regards!