This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

pcm3070-cs k 音頻總線設置不太理解

pcm3070-cs k 音頻總線設置不是很明白。問題如下:

1、音頻接口模式有I2C / DSP / left justified / right justified 其后三者有什麽用途呢?

2、BLCK Polarity 是什麽意思呢?與 BLCK Direction 有什麽關係?

3、Audio bus loopback / Digital loopback 是什麽作用呢?

  • Hi,

    1、音频接口数据格式I2S、DSP、左对齐、右对齐是针对不同的设备和协议而定义的,目的就是为了兼容不同的标准。

    2、BCLK时钟极性是指数据有效是在上升沿还是下降沿,可以选择。时钟方向用于主从设置,作为主设备时,BCLK要对外输出;作为从设备时,BCLK接受来自主设备的时钟。

    3、Loopback回环模式主要用于测试,你可以将ADC采集的数据直接送给DAC输出,验证功能是否正常。

  • Hi

               1.音频接口的标准I是I2S,在I2S下有几种模式I2S,DSP,左对齐和右对齐模式。这个根据你的需要来选择使用。比如有些DSP需要采用时分复用的接口,那就可以使用DSP模式,左对齐和右对齐最主要看你接收或者发送的器件支持哪种格式来决定。

                2.BCLK polarity:改变BCLK的极性。BCLK direction是用来选择BCLK的方向的,当Codec作为主时,要设置为输出,为从时要设置为输入。

                3.Audio bus loopback与Digital loopback主要是用来让你调试的,Audio bus loopback 是指I2S Din进,Dout出。Digital loopback 是ADC的I2S传输给DAC的I2S。一般情况下,不配置minidsp你的数据是传不到DAC或者输出的,需要通过loopback的方式将数据传输过去。