This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV595: 给TEC供电

Part Number: DRV595


想采用DRV595给TEC供电,请教几个问题:

1. 增益问题:根据手册table1,DRV595的增益从20dB到36dB,是否意味着输出电压差(OUTP-OUTN)是输入电压(IN+减去IN-)的10倍到63倍?是否可以设置更小的增益,比如增益为1倍?

2. 如果我将IN-接到2.5V,用IN+控制TEC。IN+的电压大于2.5V,电流从OUTP流向OUTN;IN+的电压小于2.5V,电流从OUTN流向OUTP,这么理解对吗?

3.  输出电压差(OUTP-OUTN)的最大值受限于输入电源电压VCC? 比如TEC所需电流1A,TEC的内阻为10欧姆,输出电压差(OUTP-OUTN)就输出10V,要求VCC也大于10V才可以?

谢谢