This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
用TLV320AIC3254做一款产品,输入信号有一路I2S,2路Line in(左右声道),看TLV320AIC3254上面支持3路Line IN和I2S输入,理论可行,目前的问题如下:
1.当1路I2S和2路line in都同时有音频输入时,TLV320AIC3254是怎么处理,可以同时输入和同时输出(混音方式)?还是只能接受一路音源?
2.如果I2S和Line in输入,是否都能做I2S输出?后面接数字功放
3.TLV320AIC3254的输出端支持LOL/LOR以及HPL/HPR,4个通道是否可做同时有音频输出?
感谢回复!
还有疑问,如果用来做两路模拟音频输入(比如:IN1_L/IN1_R & IN2_L/IN2_R)和一组I2S数字音频输入,总共3路输入,是否可配置成同时作为输入,同时HPL/HPR&LOL/LOR能配置同时输出? 另外,是否可以帮忙推荐比ADAU1401算力更强的DSP IC,需要能独立处理左右声道,还能在内部配置EQ以及加入一些滤波,信号侦测判断,还要能做信号调制等,目前使用的AUAD1401,采样192K情况下,只能加入很少的配置,就没办法动起来,超过其能处理的范围。 感谢~~
可以的,下面这个框图可以看出更详细的信号路径,是下面参考指南手册里的截图,手册中第四部分有示例代码,第五部分有详细的寄存器map说明
TLV320AIC3254 Application Reference Guide (Rev. A):
https://www.ti.com/lit/an/slaa408a/slaa408a.pdf
关于DSP IC的推荐,抱歉,TI没有相应的音频DSP 推荐给您,在TI的音频产品中,如下链接,只有音频编解码器有比较多的ADC和DAC模块
https://www.ti.com.cn/zh-cn/audio-ic/overview.html