Part Number: TAS5558

大家好! 帮分析下 TAS5558 是否可以支持两路IIS主设备同时输入?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,可以的,两路分别在bank 1 和bank 2. 通过寄存器0XC4可以对ASRC#1 和ASRC#2 都配置为I2S输入的。

您好! 我设置了OXC4 寄存器后, 两路IIS输入都有声音,但是ASRC#2输入的声音有卡顿。 我将ASRC#2输入的信号接在ASRC#1上输入声音没有卡顿现象。 我怀疑是ASRC#2的
没有MCLK输入的原因。 请问:在ASRC#1连接了MCLK的情况下,ASRC#2的MCLK是否还需要接入,还是说还有哪里设置不对?
我们两路IIS 信号都是标准的IIS, 48KHZ采样率,3.072MHZ SCK, 48KHZ LRCLK.