Part Number: TPA3255
关于TPA3255的外围电路有两个地方想请教一下。
1.下图红圈所示的接于PVDD_AB和PVDD_CD的电解电容,在TPA3255 EVM开发板上使用了4700uf容值的电容。
TPA3255数据手册上的推荐电路以及EVM开发板的电路中并未看到大电容的放电回路,
采用此量级的大电容时是否需要在TPA3255的外围电路中添加电容的放电回路?还是说TPA3255内部已做了相关的放电处理功能?
2.想确认一下下图蓝圈所标注的3.3Ω电阻的作用。
麻烦了,谢谢!