This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV612: 急急急.可调增益运放DRV612的GAIN引脚接数字电位器tpl0501不能调整增益问题

Part Number: DRV612

您好问下,单独调试tpl0501,用万用表量W和H两端电阻阻值有变化,但tpl0501的H接DRV612的GAIN引脚,tpl0501的W接地,不能控制DRV612运放的输出增益。DRV612的GAIN接固定电阻可以控制增益输出。

  • 您好,

    DRV612的GAIN接固定电阻,您测量下GAIN管脚的电压是多少?请注意,TPL0501的VH, VL端电压最大不能超过VDD;

    您DRV612的工作频率是多少?TPL0501在RHEOSTAT 模式下典型工作频率是60kHZ,检查下是否超出了TPL0501的工作频率?

  • 您好,谢谢回答。

    1、GAIN接固定电阻对地电压为0.5V,

    2、DRV612供电电压为3.3V,TPL0501供电电压为5V,会不会是TPL0501的供电电压影响DRV612?

    3、这电路我们主要用在音频前端放大电路,所以频率远低于60KHZ

    麻烦帮我们看下,这电路哪里有不对的对方,仔细看过datasheet没有感觉没有哪里不对

  • DRV612需要上电前设置好增益,因为增益设置在通电期间锁定。您在使用TPL0501调节增益时,是否对DRV612重新上电,以重新锁定新设置的增益?

    另外,DRV612的mute管脚是低电平有效,但是我看到您将mute管脚经1k电阻接地了,DRV612还有输出吗?

  • 感谢回答

    1、刚才按照上电要求,先给TPL0501上电电阻设置到4K左右,然后接到DRV612的GAIN引脚上再给DRV612上电。正常应该10倍关系,但实际量了下DRV612输出波形幅度只有输入波形的两倍。看了文档相当于GAIN引脚悬空。

    2、mute引脚下拉电阻到地,GAIN引脚悬空,正常的。

  • 关于您的第2点,不清楚您说的什么是正常的

    我从我的一个同事那了解到DRV612的增益是在VDD电压达到2.8V时设置的The gain is set when the VDD voltage reaches 2.8V.),所以请检查下VDD电压是否稳定或存在纹波,以免影响DRV612的增益设定。

    我的上一条的疑问是关于mute,DRV612的mute管脚是低电平有效,您的电路中将mute管脚拉低了,DRV612不应该有输出才对。

  • 1、不好意思,关于mute引脚,硬件工程师之前已经将这个mute引脚上拉高电平,我这原理图还未更新。

    2、硬件工程师将GAIN引脚接普通滑动电位器是可以的。

  • 使用TPL0501接入的电阻,对DRV612相当于GAIN引脚悬空,这应该是DRV612上电过程中没有锁定TPL0501设置的增益造成的,

    在使用TPL0501设置DRV612增益时,建议您用示波器测量下DRV612上电时的供电电压波形