您好!请教一下我们使用tas5558 模式1(图1), 通过 SDIN5输入模拟话筒信号。当外部声卡改成(24bit 48000 如下图2)(测量TAS5558 MCLK 为12.288MHZ,采样率为48KHZ,), 功放输出会有3-4khz一个比较固定频率噪音。
而将外部声卡改成(24bit 44100 如下图2)(测量TAS5558 MCLK为11.289MHZ,采样率44.1khz,) 没有噪音。 想咨询下,这个噪音跟TAS5558的某个寄存器设置有没有关系?
图1
图2
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好!请教一下我们使用tas5558 模式1(图1), 通过 SDIN5输入模拟话筒信号。当外部声卡改成(24bit 48000 如下图2)(测量TAS5558 MCLK 为12.288MHZ,采样率为48KHZ,), 功放输出会有3-4khz一个比较固定频率噪音。
而将外部声卡改成(24bit 44100 如下图2)(测量TAS5558 MCLK为11.289MHZ,采样率44.1khz,) 没有噪音。 想咨询下,这个噪音跟TAS5558的某个寄存器设置有没有关系?
图1
图2
这里写SDIN5需要以post-ASRC的速率工作,是不是这里D20需要设置为1:Serial clock output sampling rate is the internal sampling rate
我先去确认下这个情况
您好,我咨询了美国的工程师,他回复说与寄存器设置无关,声卡设置将影响计算机和EVM之间的连接(“This problem doesn't have connection with register settings. The sound card setting will affect the connection between computer and EVM”)。
您检查下电脑与板子的连接情况,看是哪里的问题造成的