Other Parts Discussed in Thread: TIDA-00733, , TPA6404-Q1
TAS6424 的开关频率2.MHz 在EMC CE 电压法测试中出现超标情况。请问从哪个方面可以改善呢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TAS6424 的开关频率2.MHz 在EMC CE 电压法测试中出现超标情况。请问从哪个方面可以改善呢
您好,
一般是从输出端LC滤波器着手解决,LC滤波器衰减PWM频率并减少电磁发射,LC滤波器的推荐低通截止频率取决于选择的开关频率。对于2.1 MHz的PWM频率,低通截止频率可选择最大到100 kHz。对于电感的选择,其电流值需使用电感器的电感-电流曲线,确保在系统设计提供的最大电流下,电感不会降至2µH以下(对于fSW=2.1 MHz)。电感的DCR直接影响系统设计的输出功率。DCR越低,为扬声器提供的功率越大。4Ω系统的典型电感器DCR为40至50 mΩ,2Ω系统的典型电感器DCR为20至25 mΩ。
对于LC滤波电路的设计,请参考Class-D LC Filter Design:http://www.ti.com/cn/lit/pdf/SLOA119
我看到您参考的是TIDA-00733参考设计,但是我看到其设计指南里,如下链接,如下截图部分说明,它使用的输出电感不是共模电感,是为了节省空间,采用了双电感器。每个封装中的两个电感器没有磁耦合在一起。
下面文档第5部分有关于TAS6424-Q1 EMC 设计注意事项,希望对您解决您的问题有帮助:
汽车级音频功放 TAS6424-Q1/TPA6404-Q1 设计注意事项 :https://www.ti.com.cn/cn/lit/an/zhca947/zhca947.pdf