This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好
我现在在MCU上配置这颗PCM1865芯片声音录入,有按照规格书,自己配了部分寄存器,但未能正常录到声音,请问是否有寄存器初始化样例提供
我们的mclk是外部晶振提供12.288M.
谢谢
您好,
可以提供的最接近的将是公开可用的Linux驱动程序 ,希望对您有所帮助:
PCM186x ADC family Linux driver https://www.ti.com.cn/tool/cn/PCM186X-DRIVERS
我看您BCK输出6.14M,LRCK输出48k,比率应该设置的是128。在master 模式下,仅支持以下BCK与LRCK比率:32x、48x、64x和256x,不支持128x。
通过寄存器Page.0, 0x20 bit CLKDET_EN,可以使能自动配置,您可以查看您是否使能了这位
使用 12.2288M mclk,播放44.k,应该需要配置PLL,您可以使能CLKDET_EN,看下是否可以自动的去分频
1、切换后,这里是什么现象?mic信号相对于line信号,幅值比较小,MIC时,应将增益调大些;
2、您是用什么电路在播放?这个电路播放其他音频信号效果正常吗?
1.现象是无论是否切换都用line in接入测试声音变化不大,我今天将切换的时候0x01和0x02寄存器也改变了,声音的音轨会有大的变化。不知道是否符合要求
您这里的切换具体指什么,我感觉我没太明白您的意思?
2、IOVDD可以用1.8V,也可以用3.3V,这影响数字I/O口的电平
1.切换只是硬件上做了个标志,软件去获取到,然后重新配置寄存器达到line和mic的区别而已,这个问题到不是很急
2.能否帮忙处理一下现在PCM1865给到输出DAC的声音比较沉闷,没有高音透彻的那种感觉,该如何解决。电压是有试过改为3.3确实没效果。有配过一些PGA的寄存器也没能生效,不知道哪里出了问题,能否帮忙看一下看原理图分析一下
谢谢